WTCC & CTCC Shanghai Station: SVW 333 Won The Champion Würth Booth Overwhelmed With Visitors
25/09/16
From Sep. 24th to 25th CTCC and WTCC was held in Shanghai Circuit. On June, SVW 333 took part in the competition held in Jiashan Station. Thus, this is the second time that SVW 333 has taken part in the game. Zhang Zhendong, an experienced racer, won the first place by keeping calm and using excellent skills. He overtook from the edge of the track, while there was only one millisecond narrow between him and the car behind him. He is also the champion of Manufacture Cup.
As the official sponsor of SVW 333, Würth prepared basketball game and darts for audience. The booth was overwhelmed with visitors who came to pick up gifts. Just before the final, we invited Adam Morgan, racer of SVW 333, and beautiful show girls to the booth, who talked and took pictures with audience. Nearly thousands of fans followed Würth’s WeChat. A long line was formed before the booth. Next station of CTCC will be held in Guiyang, Guizhou Province, a place famous for its rough geographic feature, which means that racers will have to embrace the challenge.